This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I will buy the EVM430-FR6047 board to try the ultrasonic transducers that I am buying from STEMINC. I want to meassure water flow through a pipe so I think the 2mm thick (1 Mhz) and 15mm radius transducer should do it. Should I take into another consideration?
Also, if I want to use the board just with batteries, how should I program it so it will stay in low battery consumption mode?
Last thing, if I want to transfer water flow meassurments from the board to a web server. What boosterPack could you recommend me? (like CC3100BOOST pack for example??)
Thanks a lot,
David.
Hi Eddie,
Thanks for the answer, I am talking now with the guys from Audiowell. But just to be sure, the transducers from SISTEMICS can not be used for flow water meters, or they just have low performance for that purpose??
Last question please, I will buy also the microcontroller (MSP430FR6047) alone because I would like to program it for a specific application. You told me that in order to program it, I will require the MSP-FET. Am I right by saying that this MSP - FET is capable of programing every MSP430xx microcontroler? (just wanna be sure I am not spending 115 dollars in one application). And also, I guess I would have to make my own PCB to connect the MSP-FET with the microcontroller (MSP430FR6047) and program it. Should I have anything else into consideration if I would like to program it?
Thanks,
David.
**Attention** This is a public forum