This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2310: 1.5V ADC Reference Specs with temperature

Part Number: MSP430FR2310


Greetings,

Looking at the device datasheet, I see a specification for "Total unadjusted Error" of +- 3% for the 1.5V voltage reference can can be fed into the ADC. I do not see any indication that this spec takes into consideration the full operating temperature range.

Do you all have a spec for total error in this 1.5V reference in the temperature range of -30C to 60C ?

Thanks

**Attention** This is a public forum