Other Parts Discussed in Thread: MSP-FET,
Hello ,
once i try downloading the program to the MCU (by clicking on debug and download button) i get the error :
i think i connected the MSP-FET emulator correctly to the MSP430.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello ,
once i try downloading the program to the MCU (by clicking on debug and download button) i get the error :
i think i connected the MSP-FET emulator correctly to the MSP430.
Hi ,
i am using a custom board that we designed .
I also use SBW connection to the MSP FET.
I already made sure that the MSP430 gets voltage its needed (above 1.8V) - so the MSP-FET supposed to find the target device.
A little background of the board :
The board is for GPS purposes , it suppposed to supply a good pulse ( 1Hz pulse) and a bad pulse ( 0.5Hz pulse) depends on various conditions.
I tried to download the code through code composer and IAR embedded ( i encountered the same error).6014.updated electrical drawing.pdf
i attached an electrical schematic of the board.
hello ,
my options are already configured that way ...
after rebuilding all i get no error...and it still pops up that error over and over again...
what could be the problem?
**Attention** This is a public forum