This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-FET430UIF: Device not detected in IAR 4.21 as Valid COM

Part Number: MSP-FET430UIF

Hi,

I'm trying to debug through IAR workbench version 4.21 and MSP-430 USB debug interface (MSP-FET430UIF). I'm using an Windows 10 64 bit machine.when i try connecting to the module using the debugger there is no COM port visible .Its something like this,

I could see the device name as MSP-FET430UIF CDC (COM 11) in the device manager.

I could see the power LED on and Mode LED blinking once or twice while i try downloading the file to the module. can you please help me with the drivers required for windows 10 for the debugger to connect the module through IAR. also can tell me the steps to be followed to change things. I could find drivers for windows 7 64 bit only , but that did not help.Can you please help in connecting the module with the machine through the debugger.

regards,

Gopal

**Attention** This is a public forum