This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everybody
please FET via USB is working fine with revD devices .
mounting same board same sw but rev F device IAR cannot recognize the device .
does this happen to you ?
suggestion ? customer would like to stay unless forced on 4.x since sw is done with that .
thank you
bye
Carlo
Hi Carlo, I remember some trouble with older silicon samples on 2005 but not with new, also nothing is reported on errata about your trouble and I moved to new 2xx.
Which version of programmer are you using? Installing in parallel a new version of compiler and try load a small piece of software recognize the device? Also check about installation try reinstall IAR from scratch or check license status.
Regards
Roberto
Ciao Roberto ,
thank you
I reinstalled IAR using latest and it is up and working !
bye
Carlo
Hi Carlo, happy see you solved the problem, please also close this question.
Old version of IAR work and there is no need to remove, still can you use previous version till don't open and save workspace with a new version.
I am using an older 4.20 and new 5.30 together on an XP vbox Linux hosted, when XP upgraded to SP3 some year ago burned out some programmer so i decided to use linux and leave old project on a clean XP SP2 free from update.
If your customer is using licensed version I understand the cost of upgrade but if code is no more than 4/8K then no reason exist to lock on 4.xx version, I also avoid use win 7 where SP3 problem are still active with new ones.
Regards (Ciao )
Roberto
**Attention** This is a public forum