This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can i still download IAR 4.21 ?



Hello...

 

I have two simple questions... either one would be helpful.

 

1. Can one still download the version 4.21 of IAR?   (I believe that this is slac050v.zip.)

2. Was that the version that shipped with the EZ430-RF2500 product?

 

Thank you for any help.

We are working on a legacy project and want to use the same version of compiler as was previously used.

 

-Sage

 

  • Hi Sage,

    1.) I'm sorry, but I have no glue! I don't think that older versions will be available on the website.

    2.) Well, that shurely depends on the data of purchase (production). I think you will need to check it out!

    Rgds
    aBUGSworstnightmare

  • If you have an IAR license and your license fees are up to date, you will be able to download any previous version of IAR Embedded Workbench for which you have a license through the IAR website.

    If you are using a kickstart or evaluation version, IAR does not make older versions publicly accessible.

  • If you have any account, this is where you login in.  It's tricky to find sometimes.

     

    From there click on your specific license and then click on "Product Update Page".  Then scroll down to the bottom of the page and click on "Other Versions". There you should find all the older versions (and their service pack updates).

    **Edit: 1-29-16 Link broke, updated.

**Attention** This is a public forum