Part Number: MSP-EXP430FR6989
Other Parts Discussed in Thread: TIDM-LC-WATERMTR, TIDM-INDUCTIVEPROX
Hello,
I am trying to make an inductive sensing of a water meter spinning wheel.
So far I tried example TIDM-INDUCTIVEPROX, which is using only one sensor. The detection with this SW was very good, how ever I need two LC sensors. So run the example TIDM-LC-WATERMTR with two LC sensor, it somehow works (not very reliable) but I can't get the sensitivity to metal as was in the example with only one sensor. I am using the same combination of C and L. I was changing the values of separation factor and distance, however the sensitivy still isn't as good as in the example with one sensor.
What else can I do to increase the sensitivity? Or should I just modify the first example to 2 LC sensors?
Thank you