This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-TS432PZ100: MSP-TS432PZ100 LDO doesn't work

Part Number: MSP-TS432PZ100
Other Parts Discussed in Thread: SEGGER, CCSTUDIO

Hi,

I received an MSP-TS432PZ100 socket board but it doesn't work.  I have tried to test with MSP432P4111 and MSP432P401R. I use Segger J-Link Pro debugger probe and power the board from the debugger(Pin 19, 5V).  The LDO SEL was used, which Pin2 and Pin3 of JP6 were connected. Finally, I checked the power on the Pin 13 of the socket, it is not a 3.3V but a 5.0V.  That means the LDO doesn't work, and it makes that chips don't work anymore. I would like to know is this a malfunction of the MSP-TS432PZ100 socket board? Or how to solve this problem?  Thank you.

Sunglin.

**Attention** This is a public forum