This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5528: BSL-Scripter with MSP-FETFlash Emulation Tool to I2C BSL-Bootloader

Part Number: MSP430F5528


Hi,

I have modified the MSP430F522x_I2C example from the "MSP430BSL_1_01_00_01.zip" to work with MSP430F5528.

I can successfully switch into BSL-Mode by using:

__disable_interrupt(); // disable interrupts
((void ( * )())0x1000)(); // jump to BSL

Now I am trying to use BSL-Scripter to communicate with the BSL and to upload new Firmware to the MSP430F5528.

Unfortunately BSL-Scripter seems to not support I2C BSL for 5xx Microcontrollers:

MODE 5xx I2C 100000 COM7
[ERROR_MESSAGE]The communication protocol chosen is not available for the chosen Family!

if just pretent to have an FR-Type, I receive a failure message but I have veryfied that the password was successfully transmitted:

MODE FRxx I2C 100000 COM7//FRxx
RX_PASSWORD .\pass_default.txt
                        Read Txt File : C:\ti\ScriptExampleWindows\test\pass_default.txt
                        [ACK_ERROR_MESSAGE]Unknown ACK value!

Is there any chance to have a BSL-Scripter.exe thtat allows I2C for 5xx?

or am I just using the wrong Family Name?

b.r.

David

**Attention** This is a public forum