Tool/software: Code Composer Studio
I´m in the middle of a project that needs to communicate two MSP430F2619, I´ve made two pcbs, one with the MSP430F2619TPM (usual), that works fine, and another one that uses the MSP430F2619SPM (high temperature rated version) which simply does not connect to CCS.
In futher inspection i realized that the TI part site says that the family user guide to use with this F2619SPM is the x5xx or the x6xx families (www.ti.com/.../MSP430F2619S-HT) which is really odd and mind boggling to me.
I´ve tried the following:
-Replace chip for a brand new one.
-Test JTAG (RST, TDI,TDO...) traces from connector to chip.
-Check voltage levels, AVcc and DVcc.
Ps.: the project needs to be HT rated, so I really need to use te SPM variant.