Other Parts Discussed in Thread: MSP-FET
Hallo,
my MSP430 firmware is designed to communicate via JTAG mailbox (JMB). I am locking for best solution to interface the JMB withe a PC just to send commands, read logging data, adjust control parameters etc...
TI provides the Application Report SLAA763 where the JMP is interfaced by a SimpleLink™ MSP432P401R MCU operating as JMB host. For connection to the PC a UART interface of this MCU can be used. TI delivers sourc code for the SimpleLink™ MCU.
On the other hand I have the MSP-FET available.
1. Is my assumption correct that the MSP-FET is able to communicate via JMB too?
2. Is there any PC-software available supporting a simple communication via MSM-FET and JMP?
3. Are there further alternatives for an adapter between my MSP430 JMB and the PC?
best regards
Stefan