Part Number: MSP-EXP430FG4618
Tool/software: Code Composer Studio
CCS can't download the code to the board.
Hi dear friend;
I have just now bought the experimenter's board with MSP430FG4618/F2013. I'll dowload code without MSP430 FET. The board supports RS232 and has a 9-pin terminal. I have tried to download some code from CCS( Version: 8.2.0.00007) by RS232 ; without MSP430 FET.
The connection from the PC to the end of the RS232 is all right, because I can see the reaction (+ and - Pulses) after I have presset " Identify" in the CCS. So I assume, the selection of the COM PORT and the setting of the UART-Connection are OK.
But CCS can't download the program and the error massage from the Launching Debug Session is: Load failed.
What else have I to do to run the Board? Any suggestion?