Other Parts Discussed in Thread: TIDM-TWOPHASEMETER-I2040, TIDM-SERVER-PWR-MON
Support,
I'm using the TIDM-SERVER-PWRMON kit and SW.
1. Verify that readings are updated every 4 AC cycles? Where in the code is this set? Can it be changed? What is minimum time needed for bg/fg processing?
2. Verify readings of specific datum (Current, Voltage, etc), are averaged? i.e. what rate will readings change if, for example the current instantaneously jumps from 5A to 20A?
3. Verify if UART GET_READINGS CMD is sent < 4 AC cycles, the data will be the same. Does too frequent UART requests impact processing? i.e. holds off new calculation data.
4. When system is started, coming out of reset, the initial current readings are high, even without LOAD. Shouldn't it be ZERO?
5. In the design document, SLAA638, 'HOST_CMD_GET_CONSUMPTION_PHASE_1' is not detailed?
6. I cannot find the the function : energy_consumed[phx][APP_ACTIVE_ENERGY_EXPORTED];
7. There is no command to 'write energy consumption data'. This would be used for a host to update energy data in the case MSP loses power and starts from zero. My intent is to write a new CMD to perform this function.
Regards,
Marc