This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi, I have a board which has an external 16Mhz crystal on XT1.
I have code which runs this board either from the internal DCO @ 16Mhz or using the external xtal.
When configured for the external oscillator i'm getting about 350uA more current when in LMP4 mode than with the internal DCO.
Is there something I should be doing to turn off the XT1 before going into LMP4?
void InitXTAL(void) { //Set Up Vcore Voltage Level 2 up to 20Mhz PMM_setVCore(PMM_CORE_LEVEL_2); #ifdef INT_XTAL //Configure XTAL IO GPIOConfigOutputLow(IO_XTAL_XT1_XIN); //XT1 Output Low GPIOConfigOutputLow(IO_XTAL_XT1_XOUT); //XT1 Output Low UCSCTL3 = SELREF__REFOCLK; // FLL: REFO UCSCTL4 = SELA__REFOCLK | SELS__DCOCLK | SELM__DCOCLK; //ACLK: REFO, SMCLK: DCO, MCLK: DCO UCSCTL5 = DIVS__2; //SMCLK: /2 UCSCTL6 = XT1OFF | XT2OFF; // turn off XT1 and XT2 // Initialize DCO to 16.00MHz __bis_SR_register(SCG0); // Disable the FLL control loop UCSCTL0 = 0x0000u; // Set lowest possible DCOx, MODx UCSCTL1 = DCORSEL_7; // Set RSELx for DCO = 50 MHz UCSCTL2 = 488u; // Set DCO Multiplier for 16MHz // (N + 1) * FLLRef = Fdco // (488 + 1) * 32768 = 16MHz __bic_SR_register(SCG0); // Enable the FLL control loop // Worst-case settling time for the DCO when the DCO range bits have been // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx // UG for optimization. // 32*32*16MHz/32768Hz = 500000 = MCLK cycles for DCO to settle __delay_cycles(500000u); #else //Ext XTAL //Config XTAL IO GPIODirInput(IO_XTAL_XT1_XIN); //Input GPIODirOutput(IO_XTAL_XT1_XOUT); //Output GPIOPeripheralEnable(IO_XTAL_XT1_XIN); //Set XIN as peripheral function which is XT1 GPIOPeripheralEnable(IO_XTAL_XT1_XOUT); //Set XOUT as peripheral function which is XT1 //Enable XT1 with mid drive strength UCSCTL6 = XTS | XT1DRIVE_1 | XT2OFF; //XTAL = 16MHz - MCLK 16MHz - SMCLK 8MHz UCSCTL4 = SELA__REFOCLK | SELS__XT1CLK | SELM__XT1CLK; //ACLK: REFO, SMCLK: XT1, MCLK: XT1 UCSCTL5 = DIVS__2; //SMCLK: /2 #endif //Make sure ACLK stays on all the time BitSet(UCSCTL8, ACLKREQEN); /* Loop until XT1,XT2 & DCO fault flag is cleared */ do { // Clear XT2,XT1,DCO fault flags (Reset if still in fault) BitClear(UCSCTL7, (XT2OFFG + XT1LFOFFG + XT1HFOFFG + DCOFFG)); // Clear Oscillator fault flags BitClear(SFRIFG1, OFIFG); } while (BitTest(SFRIFG1,OFIFG)); //Test oscillator fault flag }
**Attention** This is a public forum