Part Number: MSP430FR6989
Tool/software: Code Composer Studio
I was using the following program as i2c scanner, but the problem is that when I connect a device via i2c, the program detects it every 3 iterations but not in everyone; while a friend of mine is running the same code and it detects it every single one of them. Could it be a CCS problem? Any idea of what could be happening?
#include <msp430.h>
#include <msp430fr6989.h>
#include "utils.h"
#include "uart.h"
#include "pins.h"
#include "driverlib/driverlib.h"
#include <stdint.h>
#include <stdio.h>
int main(void){
char buff[100];
WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer
// Configure clock
CSCTL0 = 0xA500; // "Password" to access clock calibration registers
CSCTL1 = DCOFSEL_0 | DCORSEL; // Frequency of the main DCOCLK clock 8 MHz
CSCTL2 = SELS_3 | SELA_1;//DCOCLK as input CLK for SMCLK
CSCTL3 = 0x0000; // No prescalers
//Set UART and I2C pins
GPIO_setAsPeripheralModuleFunctionInputPin(OV_SDA, GPIO_SECONDARY_MODULE_FUNCTION);
GPIO_setAsPeripheralModuleFunctionInputPin(OV_SCL, GPIO_SECONDARY_MODULE_FUNCTION);
GPIO_setAsPeripheralModuleFunctionInputPin(UART_RX,GPIO_PRIMARY_MODULE_FUNCTION);
GPIO_setAsPeripheralModuleFunctionInputPin(UART_TX,GPIO_PRIMARY_MODULE_FUNCTION);
PMM_unlockLPM5();
// UART configuration
unsigned long divider =(1000000U <<4)/9600; //Do the division and with decimals (that's why we shift left)
unsigned long mod = divider&0xFFF0; // UCBRFx = INT([(N/16) -INT(N/16)] - 16) (you can check that the operation in the code corresponds to the bit stuff
divider>>=8; // remove decimals
UCA0CTLW0 = UCSWRST; // Put UART into SoftWare ReSeT
UCA0CTLW0 = UCA0CTLW0 | UCSSEL_2; // Specifies clock source for UART // aclk
UCA0BR0 = divider;
UCA0BR1 = divider>>8;
UCA0MCTLW = (unsigned char)( UCOS16 ) | mod; //use oversampling (divider > 16)
UCA0CTLW0 = UCA0CTLW0 & (~UCSWRST); // Takes UART out of SoftWare ReSeT
puts_uart0("Start!\r\n");
// i2c configuration
EUSCI_B_I2C_initMasterParam i2cConf = {0};
i2cConf.selectClockSource = EUSCI_B_I2C_CLOCKSOURCE_SMCLK;
i2cConf.i2cClk= CS_getSMCLK();
i2cConf.dataRate=EUSCI_B_I2C_SET_DATA_RATE_400KBPS;
i2cConf.autoSTOPGeneration = EUSCI_B_I2C_NO_AUTO_STOP;
EUSCI_B_I2C_initMaster(EUSCI_B1_BASE, &i2cConf);
EUSCI_B_I2C_enable(EUSCI_B1_BASE);
uint8_t addr=0;
while(1){
EUSCI_B_I2C_setSlaveAddress(EUSCI_B1_BASE, addr);
EUSCI_B_I2C_setMode(EUSCI_B1_BASE, EUSCI_B_I2C_TRANSMIT_MODE);
if(EUSCI_B_I2C_masterSendSingleByteWithTimeout(EUSCI_B1_BASE, 0x00, 10)){
sprintf(buff, "DEV FOUND AT 0x%02X\r\n",addr);
puts_uart0(buff);
};
addr++;
if(addr==0x8F){
addr=0;
puts_uart0("Round complete!\r\n");
}
__delay_cycles(100);
}
}