Part Number: MSP430L092
Hi,
I need to check the BYPASS, SAMPLE/PRELOAD, EXTEST registers are working. How to set Vector pattens for the three operations. can you help me
Thanks and Regards,
Vinothkumar.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430L092
Hi,
I need to check the BYPASS, SAMPLE/PRELOAD, EXTEST registers are working. How to set Vector pattens for the three operations. can you help me
Thanks and Regards,
Vinothkumar.
Hello Vino,
Unfortunantly, I'm not sure what the BYPASS, SAMPLE/PRELOAD, and EXTEST registers are and I don't see any reference to them in the MSP430L092 datasheet or family User's Guide. Can you clarify what you are asking?
Thanks,
JD
Hello JD,
IEEE Std 1149.1 defines nine test instructions. Of the nine instructions, three are required(BYPASS, SAMPLE/PRELOAD, EXTEST) and six (INTEST, RUNBIST, CLAMP, HIGHZ, IDCODE, USERCODE)are optional.
BYPASS= serial data to be transferred through the IC from TDI to TDO without affecting the operation of the IC
SAMPLE/PRELOAD= selects the boundaryscan register to be connected between TDI and TDO. During this instruction, the boundaryscan register can be accessed via a data scan operation
EXTEST=During this instruction, the boundary-scan register is accessed to drive test data offchip via the boundary outputs and receive test data off-chip via the boundary inputs
these are the operations Is it possible for MSP430L092?
Thanks,
vinoth
Hello Vinoth,
Understood. Unfortunately, the MSP430 does not suppost boundry scanning, with the exception of BYPASS. There is more information here: http://processors.wiki.ti.com/index.php/JTAG_(MSP430)
Thanks,
JD
Hello JD,
Thanks for your valuable replay,
I need help to do the BYPASS register, How to access the JTAG pins because one pin having (SPI_CS/TCK/P2.0/TA0.2/TA1.2/TA1.1) this designnation and how to do Bypass by using vector set.
Thanks,
vinoth.
**Attention** This is a public forum