Part Number: MSP430FR2433
Hi community member,
I have the following questions about the "DCO" and "FLL" of MSP430FR2433 .
<Background>
The customer's application is considered to be used from normal temperature environment to extremely cold environment (around -30°C).
Since the environmental temperature changes, DCO software trim is implemented. (Refer to msp430fr243x_cs7.c)
However, when the MSP430FR2433 is active mode from reset state in a very cold environment (around -30 ° C), the DCO tap will reach the maximum value of 511 at DCO initialization.
<Question>
- When the MSP430 runs in Active mode at all times, what is the recommended frequency of software trimming for the DCO?
- Please tell me the best initialization method when releasing the microcomputer reset under extremely cold environment.
- In a very cold environment, is it also necessary to change DCORSEL?
It is set as follows in DCO initialization.
- DCO frequency: 4.9125 MHz
- DCORSEL: 2
- DCOFTLIM: 4
Best regards.
Cruijff