Other Parts Discussed in Thread: MSP430F1101A
- Using MSP Gang programmer for 1st Time. uP target is 430F1101A. Programming only 1 position on 8-up board.
- Using .txt file, the unit auto programs without error.
- The target is powered by the MSP Gang. There is very little power drawn by this PCA @ 3.3V (5ma)
- There is not a capacitor on the RST line, only a 100K pullup.
- Security fuse is not blown
- I have the latest firmware loaded into the MSP GANG Programmer.
- I've moved to position 2......same thing.
Problem: Error 23 - Initialization (no communication) locks me out from any other interaction with the target device. I cannot re-program, read, Blank check, etc.
- I can still access this target device with older MSP430UIF interface running the similar, older Elpotronic software tool.
- I've messed with the power-up and reset delays...no luck.