Part Number: MSP-EXP430F5529
Other Parts Discussed in Thread: MSP430F5529
Tool/software: Code Composer Studio
Hello
i want to read ultra sonic data using msp430f5529
i found the following code it works fine
i want to know the distance value (how far is the obstacle ) i don't know how to find it in the code
please help
here is the code
#include <intrinsics.h>
#include <stdint.h>
#include <msp430.h>
#define TRIGGER_PIN BIT1 // P6.1
#define ECHO_PIN BIT3 // P1.3
#define LED_PIN BIT0 // P1.0
#define DISTANCE_THRESHOLD 60 // cm
#define MEASURE_INTERVAL 2048 // ~250 ms
void triggerMeasurement() {
// Start trigger
P6OUT |= TRIGGER_PIN;
// Wait a small amount of time with trigger high, > 10us required (~10 clock cycles at 1MHz MCLK)
__delay_cycles(10);
// End trigger
P6OUT &= ~TRIGGER_PIN;
}
int main(void) {
WDTCTL = WDTPW | WDTHOLD;
// Configure trigger pin, low to start
P6DIR |= TRIGGER_PIN;
P6OUT &= ~TRIGGER_PIN;
// Configure LED, off to start
P1DIR |= LED_PIN;
P1OUT &= ~LED_PIN;
// Configure echo pin as capture input to TA0CCR2
P1DIR &= ~ECHO_PIN;
P1SEL |= ECHO_PIN;
// Set up TA0 to capture in CCR2 on both edges from P1.3 (echo pin)
TA0CCTL2 = CM_3 | CCIS_0 | SCS | CAP | CCIE;
// Set up TA0 to compare CCR0 (measure interval)
TA0CCR0 = MEASURE_INTERVAL;
TA0CCTL0 = CCIE;
// Set up TA0 with ACLK / 4 = 8192 Hz
TA0CTL = TASSEL__ACLK | ID__4 | MC__CONTINUOUS | TACLR;
uint16_t lastCount = 0;
uint32_t distance = 0;
for (;;)
{
triggerMeasurement();
// Wait for echo start
__low_power_mode_3();
lastCount = TA0CCR2;
// Wait for echo end
__low_power_mode_3();
distance = TA0CCR2 - lastCount;
distance *= 34000;
distance >>= 14; // division by 16384 (2 ^ 14)
if (distance <= DISTANCE_THRESHOLD)
{
// Turn on LED
P1OUT |= LED_PIN;
}
else
{
// Turn off LED
P1OUT &= ~LED_PIN;
}
// Wait for the next measure interval tick
__low_power_mode_3();
}
}
#pragma vector = TIMER0_A0_VECTOR
__interrupt void TIMER0_A0_ISR (void) {
// Measure interval tick
__low_power_mode_off_on_exit();
TA0CCR0 += MEASURE_INTERVAL;
}
#pragma vector = TIMER0_A1_VECTOR
__interrupt void TIMER0_A1_ISR (void) {
// Echo pin state toggled
__low_power_mode_off_on_exit();
TA0IV = 0;
}