This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP430F5529
Tool/software: Code Composer Studio
Hello
i want to read ultra sonic data using msp430f5529
i found the following code it works fine
i want to know the distance value (how far is the obstacle ) i don't know how to find it in the code
please help
here is the code
#include <intrinsics.h> #include <stdint.h> #include <msp430.h> #define TRIGGER_PIN BIT1 // P6.1 #define ECHO_PIN BIT3 // P1.3 #define LED_PIN BIT0 // P1.0 #define DISTANCE_THRESHOLD 60 // cm #define MEASURE_INTERVAL 2048 // ~250 ms void triggerMeasurement() { // Start trigger P6OUT |= TRIGGER_PIN; // Wait a small amount of time with trigger high, > 10us required (~10 clock cycles at 1MHz MCLK) __delay_cycles(10); // End trigger P6OUT &= ~TRIGGER_PIN; } int main(void) { WDTCTL = WDTPW | WDTHOLD; // Configure trigger pin, low to start P6DIR |= TRIGGER_PIN; P6OUT &= ~TRIGGER_PIN; // Configure LED, off to start P1DIR |= LED_PIN; P1OUT &= ~LED_PIN; // Configure echo pin as capture input to TA0CCR2 P1DIR &= ~ECHO_PIN; P1SEL |= ECHO_PIN; // Set up TA0 to capture in CCR2 on both edges from P1.3 (echo pin) TA0CCTL2 = CM_3 | CCIS_0 | SCS | CAP | CCIE; // Set up TA0 to compare CCR0 (measure interval) TA0CCR0 = MEASURE_INTERVAL; TA0CCTL0 = CCIE; // Set up TA0 with ACLK / 4 = 8192 Hz TA0CTL = TASSEL__ACLK | ID__4 | MC__CONTINUOUS | TACLR; uint16_t lastCount = 0; uint32_t distance = 0; for (;;) { triggerMeasurement(); // Wait for echo start __low_power_mode_3(); lastCount = TA0CCR2; // Wait for echo end __low_power_mode_3(); distance = TA0CCR2 - lastCount; distance *= 34000; distance >>= 14; // division by 16384 (2 ^ 14) if (distance <= DISTANCE_THRESHOLD) { // Turn on LED P1OUT |= LED_PIN; } else { // Turn off LED P1OUT &= ~LED_PIN; } // Wait for the next measure interval tick __low_power_mode_3(); } } #pragma vector = TIMER0_A0_VECTOR __interrupt void TIMER0_A0_ISR (void) { // Measure interval tick __low_power_mode_off_on_exit(); TA0CCR0 += MEASURE_INTERVAL; } #pragma vector = TIMER0_A1_VECTOR __interrupt void TIMER0_A1_ISR (void) { // Echo pin state toggled __low_power_mode_off_on_exit(); TA0IV = 0; }
Hello Winter Yu and Ling Zhu2
i really appreciate your kidness
i have another question please
why to set the MEASURE_INTERVAL to 2048
and could anyone explain me the following equation i didn't get exactly how to find the distance from this equation
distance *= 34000;
distance >>= 14; // division by 16384 (2 ^ 14)
i know that distance = duration * 0.034/2;
1. You set up TA0 with ACLK / 4 = 8192 Hz, so set the MEASURE_INTERVAL to 2048 to get a 250ms measurement interval which means 4Hz sample rate. This measurement interval is based on power consumption, sample rate and minimum time per measurement requirements.
2. Since the TA0 clock is ACLK/4 = 8192Hz = 2^13, the duration is (TA0CCR2 - lastCount)/2^13. So
distance = (TA0CCR2 - lastCount)/2^13 * 34000/2 cm = (TA0CCR2 - lastCount)/2^14 * 34000 cm.
**Attention** This is a public forum