This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I am using:
After running the code to put MSP430 to sleep, I cannot connect to the device anymore. The MSP_FET Flash shows the message "Error connecting to the target: unknown device". Then, I updated the debug configuration to erase the MSP430 before flashing. Now, MSP_FET Flash shows the message "Error connecting to the target: Could not erase device memory". Can someone help me to connect to the MSP430 via MSP_FET Flash emulation tool?
code to put MSP to sleep:
__bis_SR_register(LPM3_bits)
I tried connecting to the device using MSP flasher. with the same error ''unknown device":
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.20 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...done
* Checking for available FET debuggers:
* Found USB FET @ usbmodem14301 <- Selected
* Initializing interface @ usbmodem14301...done
* Checking firmware compatibility:
* FET firmware is up to date.
* Reading FW version...done
* Setting VCC to 3000 mV...done
* Accessing device...
# Exit: 16
# ERROR: Unknown device
* Powering down...done
* Disconnecting from device...done
*
* ----------------------------------------------------------------------------
* Driver : closed (Internal error)
* ----------------------------------------------------------------------------
*/
Press any key to continue...
The hardware connection is definitely good. And, MSP-FET flasher is functional as I am able to connect to another part MSP430FR2000 using the same tool. The output from MSP-FLASHER:
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.20 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...done
* Checking for available FET debuggers:
* Found USB FET @ usbmodem14301 <- Selected
* Initializing interface @ usbmodem14301...done
* Checking firmware compatibility:
* FET firmware is up to date.
* Reading FW version...done
* Setting VCC to 3000 mV...done
* Accessing device...done
* Reading device information...done
* Loading file into device...done
* Verifying memory (Firmware.txt)...done
*
* ----------------------------------------------------------------------------
* Arguments : -w Firmware.txt -v -g -z [VCC]
* ----------------------------------------------------------------------------
* Driver : loaded
* Dll Version : 31400000
* FwVersion : 31200000
* Interface : TIUSB
* HwVersion : U 3.0
* JTAG Mode : AUTO
* Device : MSP430FR2000
* EEM : Level 5, ClockCntrl 2
* Erase Mode : ERASE_ALL
* Prog.File : Firmware.txt
* Verified : TRUE
* BSL Unlock : FALSE
* InfoA Access: FALSE
* VCC ON : 3000 mV
* ----------------------------------------------------------------------------
* Starting target code execution...done
* Disconnecting from device...done
*
* ----------------------------------------------------------------------------
* Driver : closed (No error)
* ----------------------------------------------------------------------------
Hi Darryl,
Can you share the code that you download to your MSP430 to us?
And another tool you can try is http://www.ti.com/tool/download/UNIFLASH
Ling
**Attention** This is a public forum