Part Number: MSP432E401Y
Other Parts Discussed in Thread: MMWAVEPOEEVM
Tool/software: TI C/C++ Compiler
We are working on a field firmware upgrade solution for our MSP432E project in which a new firmware image will be received via FTP and stored in a local file system that is accessible by MSP432E. The MSP432E will then read the new image from the filesystem and program it to Flash. Then we are hoping to leverage the "Flash Mirror Mode" to switch between two Flash images on the device. A few questions:
- Are there any example for this type of field upgrade solution?
- Is there a source code example for how to parse an program image created by armhex.exe? We don't want to use .out Elf files because these have a significantly larger file size.
We are using TI ARM Compiler v18.12.3.LTS
Thanks in advance.