This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P401R: SPI with DMA

Part Number: MSP432P401R


Tool/software: Code Composer Studio

I developed my project with reference to Examples/TI Drivers/spiloopback.

http://dev.ti.com/tirex/explore/node?node=AC9hN5J9IbnJPExEuCz-7Q__z-lQYNj__LATEST

Does this driver automatically use DMA for SPI communication?

Do I have to set it up separately?

What is the maximum SPI maximum speed?

It is said that the datasheet is 16MHz, what settings need to use it?

  • Hi Joonbum,

    Yes the SPI driver already utilizes DMA, you don't have to configure it separately. 

    You can use the spi params structure to configure the bit rate:

    typedef struct {
        SPI_TransferMode transferMode;       /*!< Blocking or Callback mode */
        uint32_t         transferTimeout;    /*!< Transfer timeout in system
                                                  ticks */
        SPI_CallbackFxn  transferCallbackFxn;/*!< Callback function pointer */
        SPI_Mode         mode;               /*!< Master or Slave mode */
        /*! @brief SPI bit rate in Hz
         *
         *  Maximum bit rates supported by hardware:
         *  Device Family | Slave Max (MHz)    | Master Max (MHz) |
         *  ------------- | ------------------ | ---------------- |
         *  MSP432P4      | 16 MHz             | 24 MHz           |
         *  MSP432E4      | 10 MHz             | 60 MHz           |
         *  CC13XX/CC26XX | 4  MHz             | 12 MHz           |
         *  CC32XX        | 20 MHz             | 20 MHz           |
         *
         *  Please note that depending on the specific use case, the driver may not
         *  support the hardware's maximum bit rate.
         */
        uint32_t         bitRate;
        uint32_t         dataSize;           /*!< SPI data frame size in bits */
        SPI_FrameFormat  frameFormat;        /*!< SPI frame format */
        void            *custom;             /*!< Custom argument used by driver
                                                  implementation */
    } SPI_Params;

    Thanks,

    Alexis

**Attention** This is a public forum