Hey, I am considering to use the MSP430F47177 in one of my applications however I wanted some clarification on how i can could calculate the time required for the conversion of the input signal by the sigma delta adc.
i read the user guide supplied by TI for "MSP430x4xx Family" under chapter 29 in the SD 16 operation it is stated that the SD16 module has an input modulator frequency of up to 1 Mhz does this mean that the amount of time require to convert the input waveform into its equivalent digital output is equivalent to 1/1Mhz or 1us. Basically how long does it take for the adc to begin taking a new reading?
I want to use an external multiplexer with the already provided adc, I need to find out what is the maximum number of input signals I can provide ensuring a good sampling rate on the input signal even with the external multiplexer?