This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P401R: CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP.

Part Number: MSP432P401R

Tool/software: Code Composer Studio

Hi,

I am unable to connect to the MSP432 Launchpad. 

This all is going on after two instructions are being added to the program that is PJSEL1=0x00; PJSEL0 = 0x01; after getting a problem I removed both the instructions but it is still not working. I read this so have one doubt, Is this Shared JTAG pin causing a problem?

I browsed through the forums and tried the different solutions:

one of them is factory reset. which cant be performed, if I try connecting as per user guide instructions. the below-attached error occurs.

**Attention** This is a public forum