Part Number: MSP430FR2000
HI,
Can the MSP430FR2000 FRAM cache be disabled?
If not, how do you generate code that can run with consistent timing, such as delays?
Thanks,
Kathleen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430FR2000
HI,
Can the MSP430FR2000 FRAM cache be disabled?
If not, how do you generate code that can run with consistent timing, such as delays?
Thanks,
Kathleen
That's correct.
To clarify:
Cache can't be disabled. The cache is 4 lines of 64bits each, so in theory, it is possible to execute without Cache hits (i.e. loops, jumps, etc must be larger than cache), but this might be complicated.
The limit for FRAM is 8MHz. Below that frequency, no wait states are needed so the execution will depend on CPU frequency, whether code is executed from RAM, FRAM or Cache.
Wait states are needed above 8MHz.. Execution from FRAM will be limited by wait states, while RAM and Cache can run at the maximum CPU frequency.
So, running below 8MHz, or executing critical sections in RAM might be the best options.
Regards,
Luis R
**Attention** This is a public forum