This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
I have a serious problem with the MSPFlasher program on Linux. I have used successfully the program version 1.3.10 over a long time. I had to upgrade to 1.3.20. With this version a firmware upgrade was needed. I got the following error:
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.20 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...done
* Executing FET detection sweep:
- 1: MSP-FET @ ttyACM0 (FW update needed)
- Select FET number: 1
* Initializing interface @ ttyACM0...done
* Checking firmware compatibility:
* The firmware of your FET is outdated.
- Would you like to update it? (Y/N): Y
*********************************************************
*
* Initializing Update Bootloader.
* Programming new firmware:
* |||||||||||||||||||||||||||||||||||||||||||||||||| 100%* Update failed. (R)etry/(C)ancel? C
# Exit: 49
# ERROR: Could not find MSP-FET430UIF on specified COM port
* * ----------------------------------------------------------------------------
* Driver : closed (No error)
* ----------------------------------------------------------------------------
*/
After this the flasher was unuseable and further tries did not work:
* -----/|-------------------------------------------------------------------- *
* / |__ *
* /_ / MSP Flasher v1.3.20 *
* | / *
* -----|/-------------------------------------------------------------------- *
*
* Evaluating triggers...done
* Checking for available FET debuggers:
* Corrupted USB FET firmware detected. Starting recovery.
# Exit: 49
# ERROR: MSP-FET / eZ-FET recovery failed
*
* ----------------------------------------------------------------------------
* Driver : closed (No error)
* ----------------------------------------------------------------------------
*/
Even with a new device I got the same errors. Now I have 2 not working flasher in my office. The serial number of the old flasher starts with 14... the nwe one starts with 19...
Any idea?
Hey Karl,
It's never a bother when someone is able to solve their own issue before we even have a chance to read the question!
Have a good day!
JD
**Attention** This is a public forum