Other Parts Discussed in Thread: INA126
Hi,
I have a design that has an intermittent problem. It's a hand held battery operated instrument. Occasionally, maybe 1 in 10-20 times when an external connection is made to the board, the program glitches and causes problems. The connection can for example just be a USB connection with the other end of the USB unconnected(just the wire) or a thermocouple temperature probe that is only interfaced through a bridge to the inputs of an instrumentation amplifier(INA126)There is some sort of noise being introduced and causing a problem.
I thought I solved it when I realized I used a .01uF cap for the Vcore capacitor. I changed it to a 1uF value(~2x the 470nF recommended). That didn't solve it though.
the micro uses a 32Khz for X1 and a 16Mhz for X2. Vcc is 3.1V
Two questions;
1- How critical is the value of CVcore to be 470nF,
2- What else can be causing this? It doesn't happen when the JTAG debugger is connected , so I cant easily debug it.
Thanks for any ideas.
Jerry