Part Number: MSP-FET
Other Parts Discussed in Thread: MSP-FLASHER, UNIFLASH
Hello,
I would like to program 4 devices at once in parallel. When I connect 3 MSP-FET Flash Emulation Tool to a computer, it will appear as USB1, USB2 and USB3.
When I connect the fourth MSP-FET Flash Emulation Tool, it does not appear as a USB 4 (see the picture).
I want to use programming using the command line, so I would need to see USB4 as well. Is it possible to achieve this? Or do I have to connect a maximum of only 3 MSP-FET Flash Emulation Tool?
Thank you for answer.
Best regards
Ondrej Herink