This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like to program 4 devices at once in parallel. When I connect 3 MSP-FET Flash Emulation Tool to a computer, it will appear as USB1, USB2 and USB3.
When I connect the fourth MSP-FET Flash Emulation Tool, it does not appear as a USB 4 (see the picture).
I want to use programming using the command line, so I would need to see USB4 as well. Is it possible to achieve this? Or do I have to connect a maximum of only 3 MSP-FET Flash Emulation Tool?
Thank you for answer.
Best regards
Ondrej Herink
And what about OS, are the all 4 MSP-FET's enumerated / available in OS or not? If all are enumerated / available in OS, I guess that all of them can work with msp-flasher CLI. UniFlash is not OS, so limited number of presented FET's (if something like this exist) in GUI is irrelevant.
**Attention** This is a public forum