Part Number: MSP430FR6877
Other Parts Discussed in Thread: REP430F, MSP-FET,
Hi experts,
There are cases where my customer cannot write to MSP4306877 using MSP-GANG.
When they connected the target MSP430 to the CCS, "The Debug Interface to the device has been secured" was displayed.
They are trying to initialize with BSL, but they don't initialize well.
*********Some of the logs below ***************
MODE FRxx UART 9600 COM11
//gives wrong password to do mass erase
RX_PASSWORD pass32_wrong.txt
Read Txt File : C:\ti\BSL-Scripter\pass32_wrong.txt
[ACK_ERROR_MESSAGE]Unknown ACK value!
//add delay after giving wrong password
//because the device does not give
//any response after wrong password applied
DELAY 2000
Delay 2000 ms
RX_PASSWORD pass32_default.txt
Read Txt File : C:\ti\BSL-Scripter\pass32_default.txt
BSL Password is correct!
*******************************************************************
Are the error messages listed below caused by hardware factors?
[ACK _ ERROR _ MESSAGE] Unknown ACK value!
Best Regadrs,
O.H