This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Guys
Customer asked us to confirm that his configuration will allow Firmware updates via USB (on the main controller MSP432E401Y).
USB +5V regulated to 3V3 with TPS73733DCQR to MCU
Thanks
Regards
Rodney
Hi Rodney,
From what I can find for detailed information on MSP432E401 USB, I believe the USB connections are correct, however, I'm a little confused about the ESD suppressor connections.
Let me check first with a few folks to make sure this design is good to go.
Also, didn't know if customer was aware, here is a thread about example code to invoke BSL from the application.
And link to MSP432E Simplelink BSL guide.
Hi Rodney,
C12: please change to 3.3nF.
R22, R23: consider to connect to VBUS
have a nice day
Johann
**Attention** This is a public forum