Part Number: MSP430G2313
Dear team,
My customer used the TI software Code Composer Studio 9, did the TI of ADC sample code(msp430g2x33_adc10_01.c) compiles on the MSP430G2313 chip, then they found happened many error and came from the chip default parameter,
(Like ADC10AE0, ADC10CTL1.......) as attachment.
RD also did the others sample code compiles (Like UR, TimerA and B, nomrmal I/O....)no any problem so far, only ADC happen that, please help to check TI engineer, and try to get any comments regarding the setting or coding modify needs, Thanks!
//******************************************************************************
// MSP430G2x33/G2x53 Demo - ADC10, Sample A1, AVcc Ref, Set P1.0 if > 0.5*AVcc
//
// Description: A single sample is made on A1 with reference to AVcc.
// Software sets ADC10SC to start sample and conversion - ADC10SC
// automatically cleared at EOC. ADC10 internal oscillator times sample (16x)
// and conversion. In Mainloop MSP430 waits in LPM0 to save power until ADC10
// conversion complete, ADC10_ISR will force exit from LPM0 in Mainloop on
// reti. If A1 > 0.5*AVcc, P1.0 set, else reset.
//
// MSP430G2x33/G2x53
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// >---|P1.1/A1 P1.0|-->LED
//
// D. Dang
// Texas Instruments Inc.
// December 2010
// Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
//******************************************************************************
#include "msp430g2553.h"
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
ADC10CTL0 = ADC10SHT_2 + ADC10ON + ADC10IE; // ADC10ON, interrupt enabled
ADC10CTL1 = INCH_1; // input A1
ADC10AE0 |= 0x02; // PA.1 ADC option select
P1DIR |= 0x01; // Set P1.0 to output direction
for (;;)
{
ADC10CTL0 |= ENC + ADC10SC; // Sampling and conversion start
__bis_SR_register(CPUOFF + GIE); // LPM0, ADC10_ISR will force exit
if (ADC10MEM < 0x1FF)
P1OUT &= ~0x01; // Clear P1.0 LED off
else
P1OUT |= 0x01; // Set P1.0 LED on
}
}
// ADC10 interrupt service routine
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR(void)
{
__bic_SR_register_on_exit(CPUOFF); // Clear CPUOFF bit from 0(SR)
}
Thank you.
Kane