This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I'm in the process of migrating our firmware code to a MSP430FR5994 micro controller, everything was going rather fine until I activated the main clock with an external 16MHz quartz.
After searching for a day or two, the issue boils down to this problem : when I activate an SMCLK divider, writing to FRAM doesn't happen any more.
I've written a small piece of code (attached below) to illustrate the problem:
The result can easily be checked by displaying the (info) memory area at 0x1800, and so far this works as a charm. However, if I step further:
Nothing is written to FRAM.
I have tried this on two MSP-EXP430FR5994 boards with consistent results.
If I replace the DIVS__2 with DIVM__2, everything is OK.
I have found no indication on such a (known) bug...
So, what's happening here ?
#include <msp430.h> #include <stdint.h> /** * main.c */ void test() { uint8_t i; for (i=0; i < 255; i++) *((uint8_t *)0x1800 + i) = i; } void clear() { uint8_t j; for (j=0; j < 255; j++) *((uint8_t *)0x1800 + j) = 0xff; } int main(void) { CSCTL0 = CSKEY; CSCTL1 = DCORSEL | DCOFSEL_4; test(); clear(); CSCTL3 = DIVM__2; test(); clear(); return 0; }
So ? It works at 16Mhz, not at 8Mhz, quite the contrary of what you seem to suggest.
It works with or without DIVM at any frequency, it does not work with any DIVS (neither /2 nor /4). And by the way I can't see why it would not work if the frequency involves wait states.
The maximum MCLK frequency is clearly stated in the data sheet and the family guide covers operation of the FRAM controller in detail. This is not a mystery.
Sorry but I can't get see your point.
My issue is with SMCLK, not with MCKL. Furthermore it works perfectly well at 16Mhz. So I simply can't relate what you say to my issue, can you clarify ?
>
CSCTL3 = DIVS__2; // (per text)
This sets DIVM=0, which runs MCLK=16MHz, which (as David pointed out) is too fast with NWAITS=0. I suggest you set a breakpoint at the second line of main() to see if the CPU is reset-ing.
I also don't see where you stop the Watchdog. That could be interfering with your test. That breakpoint will also catch the reset if it happens.
So, why this works at 16Mhz DCO without wait states and no MCLK divider is mystery, but off-specs, why it doesn't work anymore with a SMCLK divider is even more unclear. Simply adding a wait state with :
FRCTL0 = FRCTLPW | NWAITS_1;
fixes the issue.
I wasn't aware the wait states need to be set manualy, thanks to David helping.
DIVM=3 (/8) at reset, so everything was fine until you set DIVM=0. [Ref User Guide (SLAU367O) Table 3-7]
**Attention** This is a public forum