Hello,
I understand from slaa666a section 5 that TI advises that when migrating from 6779 to 6779A a code recompile is required with the relevant headers. However I do not have the code and am working with an older machine which has 6779.
Is it possible that burning the hex file for 6779 Rev C. -
- Will work on 6779A? Assuming AUX PMM has not been used? Is in use?
- Will work on 67791? Assuming AUX PMM has not been used? Is in use?
- Will work on 67791A? Assuming AUX PMM has not been used? Is in use?
The intent here is should I order the easily available 6779A or 67791A or wait a couple of weeks and get the 6779.
Thanks.