Other Parts Discussed in Thread: OPA836, TIDM-02003, OPA607, OPA357, TIDA-01486, OPA838
Hi,
I am currently finishing the design of the input stage for MSP430FR604*.
It looks as on the image below:
The transducers are operated at 1MHz, sampling at 4MHz.
I have a few questions:
-
Which op-amp (U1) would you recommend for best zero flow performance? The candidates that I am currently looking at are OPA836 (as in the gas reference design TIDM-02003), OPA357 and OPA607. The gain is about 5.
-
Considering that I want a cutoff at around 2MHz, what are the optimal values for R11 and C26?
As far as I understand, this should be dependent on the ADC properties, but I could not find them on the datasheet.
On the TIDM-02003 they are 499 and 680pF (470kHz), but on the TIDA-01486 the capacitor is not present, only an input resistance of about 15Ohm (10 + 5 from the switch).
C36 should still remain 1nF, right?
Best regards,
Kostyantyn