This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This was originally posted in the "Other Microcontrollers" forum - with no response.
I have the BoostXL-Sharp128 booster pack which I'm using with the MSP430F5529 LaunchPad. Specifically I want to find example code for this booster pack. So far using Resource Explorer and looking under MSP430Ware or SimpleLink I'm not finding any. I specifically need example C code for using the microSD card. Where is the example code for this board?
Well, it isn't for that particular device and it isn't in C but I do have code for the LCD display and SD card:
Hey Ted,
I don't see any Sharp-128 examples for the MSP-EXP4320F5529LP specifically, some of the display examples on more powerful devices moved to the BOOSTXL_K350QVG-S1 touch screen LCD.
For the Sharp-128, I see in the graphics library, there are examples for MSP430G2 and FR5969 lanchpads near the bottom of the list: https://dev.ti.com/tirex/explore/node?node=AIovtMW57JlImd3Mrj9.wA__IOGqZri__LATEST
Hope these help!
JD
Hey Ted,
I also just responded to your other thread, although I probably should have combined them.
Hopefully one of the examples is what you are looking for.
Thanks,
JD
**Attention** This is a public forum