Other Parts Discussed in Thread: MSP430FR2355
Hi there,
Would need your guidance here:
I am considering the MSP430FR5729IRHAT in a new project. Is this still a good alternative or do you suggest something else?
Requirements:
- Two Timers with PWM outputs (PWM frequency 50 kHz).
- Two SPI interfaces (one slave, one Master).
- About 10 GPIO pins (few with interrupt capability).
- Support for 3.3 V supply voltage.
- Frequency > 8 MHz.
- Internal crystal preferred.
- Flash memory at least 16kB (FRAM preferred), some SRAM.
Possibly a 2 channel ADC, 8 bits minimum.
Looking forward to your comments!
thanks