This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are debugging DRV8412 board. But I found DRV8412 went to following damage status sometimes:
The first output channel (Pin5-7) is abnormal - No PWM output. But the second output channel (Pin15-17) is normal output with PWM we control. The FLT and OT are both in high level status.
So far we have found 3 pcs of DRV8412 with this same issue.
Could you help analyze which factor or operation trigger this issue? The solution will be very helpful and critical for our risk retirement. I attached circuit as below.
Thanks.
Xulong
Hello Xulong,
Pin5, 7, 15 and 17 are input pins. Do you mean OUT_C and OUT_D don't follow Pin 5 and Pin 7 PWM input?
I saw BST_x capacitor is 1uF. On the datasheet, the value is 100nF. Would you change four BST_x capacitors from 1uF to 100nF?
Regards,
Wang Li
Hi Wang Li,
Thanks for your response. Yes, I mean OUT_C and OUT_D don't follow Pin 5 and Pin 7 PWM input and I suspect the DRV8412 was damaged.
As for the BST capacitor, we have to use 1uF because our control frequency is 1kHz and I check the datasheet which described 1uF should be ok for this application:
For applications with lower than 10-kHz switching frequency and not to trigger BST_UVP protection, a larger
bootstrap capacitor can be used (for example, 1-μF capacitor for 800-Hz operation).
We use CBC mode.
Thanks.
Xulong
Xulong,
A quick look at your schematic shows that you did NOT add the series 5 ohm resistors as recommended in the datasheet for larger Bootstrap capacitors. The statement below is right after the statement you make above.
When using a bootstrap cap larger than 220 nF, it is recommended to add 5-Ω resistors between 12-V GVDD power supply and GVDD_X pins to limit the inrush current on the internal bootstrap circuitry
Without these capacitors, you risk damaging the internal bootstrap circuit.
Regards,
Ryan
Yes, I knew that and I tried adding 5-ohm resistors between 12V and GVDD. But it doesn't work. Meanwhile, when I remove C248/C386/C385/C387, the failure rate is very low, but I still found a pcs of DRV8412 is damaged after running 12 hours in our real application. So I don't think it's a great way to resolve this issue.
By the way, I still have one more question: why are all damaged channel pin5/6/7 channel (OUT_C&OUT_D) in all damaged DRV8412? The pin15/16/17 channels of all damaged chips are still very good. Could you please help give me some internal circuit mechanism explaining?
Xulong,
"I tried adding 5-ohm resistors between 12V and GVDD. But it doesn't work"
Do you mean the damage still same? Or, do you mean DRV8412 doesn't work.
"why are all damaged channel pin5/6/7 channel (OUT_C&OUT_D) in all damaged DRV8412?"
Are the Pin5, 7 input signals same as Pin15, ,17?
"when I remove C248/C386/C385/C387, the failure rate is very low,"
What is the output current? Would you share the part number of L36, L39, L45 and L47?
Regards,
Wang