This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
Here's an issue from the customer may need your help:
The motor speed cannot be increased to around 5000. With a 5V 150mA supply, increasing the supply voltage or increasing the duty cycle, the motor will stop spinning, what is the reason for that? Is it related to the DRV11873 's speed limited or the output current is out of range? Could you help check this case? Thanks.
Best Regards,
Cherry
Hi Cherry,
Can you set FS = 1? What is the PWM frequency used?
Can you set the supply to higher than 150-mA? If there is not enough current, supply can brown out to under 4.1V and this will shut off the device.
Thanks,
Aaron
Hi Aaron,
Thanks for your support here!
FS is pulled up to 5V and can reach a maximum of 9500 turns. But by increasing the voltage or duty cycle, the motor speed can no longer increase and will simply stop.
Voltage: 9V, enough current, 20K PWM frequency. Can the speed be increased more?
Thanks and regards,
Cherry
Hi Cherry,
You could be coming across a false lock condition, similar to this thread. Does this help?
https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/691434/drv11873-the-speed-issue-9000rpm-10800rpm
Thanks,
Aaron