This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Recommended Maximum GVDD and VDD operating condition is 13,2V.
Normally i would expect Absolut Maximum Rating to be somewhat higher. For example about 15V or so.
Is there a failure in the datasheet and if it is what would be the correct absolute maximum rating?