This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8316C: Current limit

Part Number: DRV8316C


Hi team,

Could you please let me confirm the current limit function?

In datasheet VILIM is limited from AVDD/2 ~ AVDD/2-0.4V, what will happen if I set it beyond AVDD/2-0.4V?

Do I need set Gain to 0.15V/A and VILIM to AVDD/2-0.4V to set 8A max?

Also, How should I handle SOX pins if I do not need to use them? Can I leave them open?

Best,
Zeming