Other Parts Discussed in Thread: DRV8320,
We are comparing data(absolute maximum rating) of DRV8320 and DRV8350.
We have three question.
①Could you tell me why is absolute maximum rating of GHx pin voltage (Vvcp+0.3V) lower than the same as DRV8320(Vvcp+0.5V)?
②Could you tell me why is absolute maximum rating of GHx pin voltage with respect to SHx (16V) higher than the same as DRV8320(13.5V)?
③ Let me know transiently (ex. under 50ns) absolute maximum rating of GHx pin voltage with respect to SHx ?