Other Parts Discussed in Thread: MCF8329A, , MCT8316A
Hi,
I have a problem with the motor driver after a power reset. I am using an Arduino to control the driver. I can read and write to all registers and I do get the motor running ok.
However;
When I keep the logic supply to the arduino and motor driver VREG to 3.3V from the arduino 3.3V regulator using an USB cable from my laptop and do a motor power reset, the system works fine, no issues. But when I disconnect the whole system and let it run of its own power source, which is all powercycled at the same time since the 3.3V is generated from the 12V source, the communication bus on the motor driver crashes. This means I cannot use a communication command to reset the ic. And if I understand there are no available hw reset pins on the driver ic!?!
Two questions arise;
1. What could be the reason for the motor driver ic to crash completely on a power up, and how can I solve this?
2. I have not connected VREG and AVDD together since I use an external 3.3V supply. COuld this be an issue?
I am super stuck. All help appreciated!