This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8212: Is there any motor driver which has a function of load monitoring?

Part Number: DRV8212


Tool/software:

Dear TI experts,

My customer tests DRV8212, but they have a problem because they cannot see the current load of motor driver.

Is there any motor driver which has a function of load monitoring when it is working?

Supply voltage to the motor is 3V~4V, operating current of motor is about 20mA~50mA.

Bigger gain is preferred. (Big voltage change is detected even in small current changes.)

Best regards,

Chase