Hi there,
I'm try to control a motor using an Android device in conjunction with an IOIO board and the DRV11873EVM. I removed the R5 resistor so I can provide an external PWM signal. However, the motor always starts at high RPM when I supply power to the IOIO as shown in this video:
http://youtu.be/u5Wh8hlrUEU
Will it be possible to use the FG pin to control the speed of the motor at startup? In other words, I need the motor to wait until the Android app has stablished communication with the IOIO board and commands it to spin.
Thanks!