Hi,
I am using the DRV8307 to control a 100W BLDC Maxon motor at 24V (http://www.maxonmotor.com/maxon/view/category/motor?target=filter&filterCategory=ecflat). My problem is: when I start the motor with the PWM signal coming from the microcontroller, sometimes the motor starts fine, but most of the times the rotor gets locked and motor do not start spinning (current rises and a lot of audible noise is generated). Why this happens? Am I doing something wrong with hall sensors connections or something? I am attaching here my schematic (the part that matters). The problem is not the motor, I have tried several different new motors.
I will appreciate any help.
Thanks in advance,