This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is using DRV8711.
He has SPI issue at customer's board.
It is different in registers setting(writing) value and reading value.
This is the issue which rarely happens.
Now, I am confirming to customer to give me SPI waveform at issue.
Could you advice me about this issue, please?
Is there SPI caution of DRV8711 only?
Best regards,
Shimizu
Hi Wilson,
Thank you for your support.
I got waveform at this issue of TORQUE bit.
Please see the attached file.
Customer has issue at MODE bit and TORQUE bit.
SPI speed is 3.4bps.
Could you advice me the cause of this issue, please?
DRV8711.pptx
Regards,
Shimizu
Hi Wilson,
Thank you for your support.
Customer found this issue by motor behavior.
Customer has this issue at MODE bit and TORQUE bit.
MODE bit changes step. TORQUE bit changes full scale chopping current.
For the this reason, customer noticed this issue immediately.
After this issue, customer added read/rewrite program to MCU.
I think cause of this issue is not Dout buffer from above.
Also, This issue has at 1Mbps, too.
Please the following picture.
I will confirm about noise.
Thanks
Shimizu
Hi Wilson,
Thank you for your support.
I will confirm detail of changing soft ware and PCB Layout.
About the below question, Is there caution?
>During operating motor(output PWM signal to motor), Is there timing-like caution against writing register? In particular torque and step setting.
Thanks
Shimizu
Hi Shimizu,
There is no any timing-like caution here. I'm working on some board with DRV8711 and actually I can change everything on the fly, such as current level(torque), decay modes, micro-stepping modes. Maybe there is noise affecting the SPI in customer board, so we need to check the layout.
Best regards,
Hi Wilson,
Thank you for your support.
I understand the following.
- There is no any timing-like caution about writing of MODE bit and TORQUE bit.
- When you try to reproduce this issue, This issue did not occur at your bench.
I don't send PCB layout to you. Please don't worry.
Thanks,
Shimizu