This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
My customer used DRV8844 to drive solenoids, but in their board they will use 16 pcs DRV8844, each DRV8844 need to drive 4 channels solenoids. every channel will consume 0.8A current. if all these solenoids work, the total current will be close to 50A. So, they came out a solution, to input PWM on EN pin , which will lead to Intermittent current flow through the solenoids, then dramatically reduce the total current. and they have to keep a small current flow through the solenoids periodically due to maintain a certain torque. Also I was told the PWM signal will be 100Khz. please kindly give your suggestion is this a feasible solution? welcome your idea for this case?
BTW, they will power DRV884 with +-24V [ dual power rails], each output pin of DRV8844 will connect to a solenoids, then to ground.
Yue,
PWM signal on EN pin to reduce the solenoid current consume should work with 100kHz PWM frequency.
I thought PWM signal on INx before. After check the ENx and INx pin delay spec, I agree PWM signal on ENx pin should work.
Please check the solenoid. Is it 24V or 48V rating? When you apply +24V to VM and -24V to VNEG, the solenoid will get 48V. Also, we may need to think about the current balancing between +24V and -24V output when they are in series.