Other Parts Discussed in Thread: TPS25750
Hi Team,
There is a Japanese customer who only has Gmail and can't post in our E2E, so I post here instead of him for help.
The customer now uses USB PD-CHAG-EVM-01 to evaluate USB PD, but it doesn't work well.
Although it is planned to implement patch bundle, it is not going well.
When purchasing USB-PD-CHG-EVM-01, it seems that it has been written into EEPROM, and 9V / 3A during operation is set to work as sink.
'BPMS' was sent to switch this, but an error occurred.
Because the mode is always APP, send "GO2P" first to switch the PTCH mode
This can also go error.
By the way, the customer uses USB-PD-CHG-EVM-01 to connect to the ARM board which is purchased in the market.
Run in the test program.
Do you need any pictures or screenshots to analyse this issue?
Hope to get your advice.
Thank you!
Regards,